I’m working on low-power mode and wakeup and have read application note “AN12245—Power Consumption and Measurement of i.MX RT1060”, along with the “MCUXpresso SDK Reference Manual_MIMXRT1060”, but I don't see where either explains how to put the MCU into low-power SNVS mode.
Also, I'm assuming that setting GPIO5, pin 0, as an interrupt (rising edge for my hardware) is sufficient for waking up the processor to run in Full-Speed Run mode. Is that the case?
I'm using MCUXpresso 11.01 for the MIMXRT1062DVJ6A, and MCUXpresso SDK USB Stack, Rev. 10, 06/2019.
Solved! Go to Solution.
Hello,
One can find the detail information for the question as the link https://www.nxp.com/docs/en/application-note/AN12085.pdf . Hope it help you.Have a nice day.
Hello,
One can find the detail information for the question as the link https://www.nxp.com/docs/en/application-note/AN12085.pdf . Hope it help you.Have a nice day.