MCUXpresso SDK for Kinetis K60 120 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso SDK for Kinetis K60 120 MHz

979 Views
BTaylor
Contributor III

Has anyone ported (and made available) the MCUXpresso Kinetis K60 100 MHz SDK code for use with the K60 120 MHz (e.g. MK60FN1M0VLQ15)?

I need to develop a serial bootloader for several custom K60/120MHz-based boards and I would like to use the MCU Bootloader framework to do so. 

0 Kudos
2 Replies

706 Views
g_lowes2
Contributor II

Hi, I would also like to use the MK60F120M0VLQ12 using MCUXpresso. I have used the TWR-K60D100M SDK which compiles on my MK60F120M0VLQ12 board by selecting MK60DN512LQ10. I have currently compiled a program which toggles a GPIO using the PIT timer. The timing does not look right, I have tried to set to 1 second intervals but seems to be slow at around 2.5 seconds. I realise I will need to modify the SDK to be fully compatible with the MK60F120M0VLQ12 board and would like to request advice on how to achieve this?

It would be great if the 120MHz Kinetis boards were supported in MCUXpresso as I have seen many other requests for this on the NXP forums.

Thanks

Gavin

0 Kudos

968 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BTaylor 

I have not heard about any porting  or plan to support MK60F120M in MCUXpresso SDK

 I think that the user that makes this porting task could take as reference the Kinetis 100 MHz Rev 1.x to 120 MHz Migration Guide

However In the TWR-K60F120M product page there is a Kinetis 120MHz bare metal sample code. that may help you.

All the best,

Diego.

 

0 Kudos