MCU ISO11898 report

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU ISO11898 report

596 Views
hma4
Contributor I

Do you have a ISO11898 conformance test reoport for the MC9S12XHY256RMV1 MCU?

0 Kudos
Reply
1 Reply

543 Views
lama
NXP TechSupport
NXP TechSupport

Hi, 

ISO11898 is the standard on the CAN 2.0 standard.

ISO 16845-1:2016 specifies the conformance test plan for the CAN data link layer and the physical signaling as standardized in ISO 11898‑1. This includes the Classical CAN protocols as well as the CAN FD protocols.

https://www.iso.org/standard/59166.html

The device is a member of S12XE devices with the same MSCANV3 CAN module. The test was performed on the "master" device of the family.

I'll sent you the CAN conformance test in parallel way.

Best regards,

Ladislav

0 Kudos
Reply