MCU-BOOT middleware missing from New Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU-BOOT middleware missing from New Project

560 Views
ivekengineer
Contributor III

I recently downloaded SDK 2.6.0 for an MKV58 device.  When I built the SDK, I chose the mcu-boot middleware component.  The component is in the SDK zip file.  However, when I attempt to create a New Project using MCUXpresso, MCU-BOOT is not an available middleware component to select.

Obviously, I can build my own generic project and use the source code to achieve what I want, but I seem to remember this being a managed component option in the past?  is this a bug, or is the middleware component only available as source code that I have to manually import?

0 Kudos
1 Reply

472 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ivekengineer,

I need to consult this with our SDK team and will update this thread as soon as I have their feedback.

Best Regards,

Robin

0 Kudos