Lauterbach connection to 8MPLUSLPD4-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lauterbach connection to 8MPLUSLPD4-EVK

3,349 Views
Ranjit131185
Contributor I

I want to use Lauterbach debugger for Flashing & debugging the M7 core.

1. Required script for M7 core of IMX8MP-EVK,

2. connection details between Lauterbach & MX8MP-EVK

Could you please help me to get the details regarding How to connect / use Lauterbach for flashing & debugging M7 core of IMX8MP EVK

 

Thanks,

Ranjit

0 Kudos
Reply
9 Replies

2,872 Views
steffendoster
Contributor IV

Hi, I have the same problem and can't connect to the 8MPLUS-BB Board (and also not to my own custom made board).

I think I connected it correctly, but I'm not able to Attach via Trace32. Tried support from Lauterbach and they gave me a new installation with iMX8MP demo script, but they fail also.

All I get is: "debug port time-out at UNKNOWN"

I built an Adapter connected like this

Lauterbach:                       i.MX8:
Pin  Description                 Pin  Description
1      VTREF   --------------   1      VTREF
2      NC
3      TRESET --------------   10    RESET
4,8,10,12,14,16,18,20        3,5,7,9
        GND       --------------           GND
5      TDI         --------------    8     TDI
7      TMS       --------------    2     TMS
9      TCK        --------------    4     TCK
13    TDO        --------------    6     TDO

Is this correct? Or what am I doing wrong?
Are there any better scripts for attachment to i.MX8 Eval board?

Greetings

Steffen

0 Kudos
Reply

3,247 Views
Ranjit131185
Contributor I

MX8MP-EVK & Lauterbach photos are shared above.
Could you please help me for Hardware connections?

0 Kudos
Reply

3,229 Views
joanxie
NXP TechSupport
NXP TechSupport

I already posted, but I don't know why community doesn't show it, you can connect to the board 10-pin debug port

 

0 Kudos
Reply

3,207 Views
Ranjit131185
Contributor I

Yes We have connected the 10 pin connector to debug port.

After power on board is in Power down mode.

 

 

Ranjit131185_0-1648128789560.png

We have selected CPU - M7, JTAG CLK = 10Mhz and then try to detect by clicking on DETECT button.

Its showing below error as Debug Port Failed.

Ranjit131185_2-1648129220484.png

 

0 Kudos
Reply

3,162 Views
joanxie
NXP TechSupport
NXP TechSupport

1. Connect Lauterbach JTAG connector to JTAG pins Header from iMX8MP baseboard.

2. Configure DIP Switches for Serial Download Mode.

3. Power on the Board

4. Start Trace32 for ARM64

5. Run xx.cmm script

 

0 Kudos
Reply

3,230 Views
joanxie
NXP TechSupport
NXP TechSupport

I already posted, but

 

0 Kudos
Reply

3,332 Views
joanxie
NXP TechSupport
NXP TechSupport

I send it to you by mail, pls check it

 

0 Kudos
Reply

3,309 Views
Ranjit131185
Contributor I

I want to know the hardware connection details between Lauterbach & MX8MP-EVK.
Once connection done, I will use .cmm files which are shared on mail.
MX8MP-EVK & Lauterbach photos are shared below.
Could you please help me for Hardware connections?

LauterbachLauterbachIMX8MP-EVKIMX8MP-EVKLauterbachLauterbach

0 Kudos
Reply

3,290 Views
joanxie
NXP TechSupport
NXP TechSupport
 
0 Kudos
Reply