LPCXpresso54628 SD card example missing from SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso54628 SD card example missing from SDK

1,300 次查看
donaldswearinge
Contributor I

I see a number of references in the forum to an SD card example in the LPCXpresso54608 SDK 2.2 named "sdcard_fatfs".

I'm using the LPCXpresso54628 board with MCUXpresso v11.0, and installed SDKs LPCXpresso54608 2.6 and LPCXpresso54628 SDK 2.6.

Neither of the 2.6 SDKs includes the sdcard_fatfs example. Has this example been removed at some point? And, if so, 1) why?, 2) are there alternative examples available?

The SDKs include a great number of useful driver examples, but this seems an odd omission for dev boards that include the SD card slot. 

0 项奖励
回复
2 回复数

1,218 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Donald Swearingen ,

 I just download the SDKv2.6 package for LPCxpresso54628, it still includes this demo "fatfs_sdcard", you can find in the path:

pastedImage_1.png

And pay attention, please select FatFS when download SDK package: 

pastedImage_2.png

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,218 次查看
donaldswearinge
Contributor I

Hi Alice,

Thanks. Yes, this is what I needed. When I first downloaded the SDK, I

was following instructions for setting up and I just took the defaults.

I was not aware that I could add other items to the SDK.

Best regards,

Donald Swearingen

0 项奖励
回复