LPC546xx - CLOCK_GetFlexCommClkFreq - Error report

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx - CLOCK_GetFlexCommClkFreq - Error report

1,387 Views
guillaume-b
Contributor I

I would like to report an error in "CLOCK_GetFlexCommClkFreq function" of "fsl_clock.c" for LPC546xx.

Below my correction :

/* Get FLEXCOMM Clk */
uint32_t CLOCK_GetFlexCommClkFreq(uint32_t id)
{
    return (SYSCON->FCLKSEL[id] == 0U) ? CLOCK_GetFro12MFreq() :
           (SYSCON->FCLKSEL[id] == 1U) ? CLOCK_GetFroHfFreq() :
           //(SYSCON->FCLKSEL[id] == 2U) ? CLOCK_GetPllOutFreq()  : // original error !!!
           //(SYSCON->FCLKSEL[id] == 3U) ? CLOCK_GetI2SMClkFreq() : // original error !!!
           (SYSCON->FCLKSEL[id] == 2U) ? CLOCK_GetAudioPllOutFreq() : // my correction
           (SYSCON->FCLKSEL[id] == 3U) ? CLOCK_GetMclkClkFreq() : // my correction
           (SYSCON->FCLKSEL[id] == 4U) ? CLOCK_GetFreq(kCLOCK_Frg) : 0U;
}

Reference : UM10912 -> 7.5.37 Flexcomm Interface clock source select registers

0 Kudos
Reply
1 Reply

1,171 Views
jeremyzhou
NXP Employee
NXP Employee

Hi BOSSARD Guillaume,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

Thanks for your reporting, and I'll transfer it to SDK software team.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply