Keil create many errors with SDK 2.3.0 for LPC54628

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keil create many errors with SDK 2.3.0 for LPC54628

2,127件の閲覧回数
salihkucukbayra
Contributor I

I can't use SDK with Keil "Manage Run-Time Environment". Build action not complate, create many error. 

"C:\Keil_v5\ARM\PACK\NXP\LPC54628_DFP\2.3.0\drivers\fsl_clock.h(689): warning:  #66-D: enumeration value is out of "int" range kNONE_to_NONE = 0x80000000U,"

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetPLL (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetUsbPhy (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetVoltageForFreq (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol main (referred from __rtentry2.o)."

Another problem for Phy chip. "Manage Run-Time Environment" suggest ethernet Phy with spi or serial. I can't select on board ethernet interface with Lan8720. This chip is behaving like no ethernet.

0 件の賞賛
返信
2 返答(返信)

1,693件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Salih,

Which SDK example project are you trying to compile? Does this happen with a specific demo?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

1,693件の閲覧回数
salihkucukbayra
Contributor I

Hi Carlos,

Example project are working. Get compile error message when I using MDK5 Manage run-time environment. 

Regards,

Salih

0 件の賞賛
返信