Keil create many errors with SDK 2.3.0 for LPC54628

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Keil create many errors with SDK 2.3.0 for LPC54628

2,076 次查看
salihkucukbayra
Contributor I

I can't use SDK with Keil "Manage Run-Time Environment". Build action not complate, create many error. 

"C:\Keil_v5\ARM\PACK\NXP\LPC54628_DFP\2.3.0\drivers\fsl_clock.h(689): warning:  #66-D: enumeration value is out of "int" range kNONE_to_NONE = 0x80000000U,"

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetPLL (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetUsbPhy (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol POWER_SetVoltageForFreq (referred from fsl_clock.o)."

".\Objects\dff.axf: Error: L6218E: Undefined symbol main (referred from __rtentry2.o)."

Another problem for Phy chip. "Manage Run-Time Environment" suggest ethernet Phy with spi or serial. I can't select on board ethernet interface with Lan8720. This chip is behaving like no ethernet.

0 项奖励
回复
2 回复数

1,642 次查看
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Salih,

Which SDK example project are you trying to compile? Does this happen with a specific demo?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

1,642 次查看
salihkucukbayra
Contributor I

Hi Carlos,

Example project are working. Get compile error message when I using MDK5 Manage run-time environment. 

Regards,

Salih

0 项奖励
回复