KL28Z SDK version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL28Z SDK version

1,386 次查看
benwang
Contributor II

We used the NXP web tool SDK builder to get the latest SDK packages on TWR or FRDM. We find the latest for KL28Z  is SDK_2.5.0, so not the same latest version as others of SDK 2.7.0. Does SDK 2.7.0 for KL28Z is still under development? If so, when will it be released public? 

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,319 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

This version is stable. So we do not update the version. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,319 次查看
benwang
Contributor II

Hi Da,

    Thanks for reply. The latest SDK version 2.5.0 used for KL28Z is released at 2018-12-17. But the version used for KL27Z is 2.7.0 is 2019-12-19. So do we have plan to update KL28Z to 2.7.0? Since we are going to migrate products from KL27Z TO KL28Z, so we have to use the same SDK version as KL27Z. Thanks

0 项奖励
回复

1,319 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Actually, we may not go on updating the kl28z.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复