Hello
I have a question
I am working with IAR, it generates an error, where I can define my micro controller MK22FN128VLL10 and how to do it, I thank you very much
Hi Oswaldo Tovar,
Please find the MK22F12810 related files in MCUXPresso SDK folder(...\SDK_2.6.0_MK22FN128xxx10\devices\MK22F12810)
CPU_MK22FN128VLL10 should define in Defined symbols.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank you, novice
I am trying to edit the clock_config file to manually select which clock source will be used. In other words, I will write conditions in the clock_config file to have options from the different clock sources. I'm supporting MCUXpresso, but there are many variables to modify, edit modes of operation, dividers and more I'm not sure if the file fsl_clock are those condition, thank you.