Is available source code to evaluate TFLM classification model with C/C+ in PC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is available source code to evaluate TFLM classification model with C/C+ in PC?

929 次查看
nnxxpp
Contributor IV

I have read tflm_cifar10 in SDK. In general, we need to convert Tflite model into C array. Now I want to evaluate TFLM model (C array, not .tflite model) in the PC to see whether accuracy is dropped. The reason I want to run in PC to save time. Do you have any source code for classification model such as for Cifar10? 

I move from Python to C/C++ and something is not familiar. Thank you.

0 项奖励
回复
2 回复数

887 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nnxxpp ,

 

Are you looking for some method like below?

https://www.tensorflow.org/lite/microcontrollers/build_convert#convert_to_a_c_array

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

884 次查看
nnxxpp
Contributor IV

@Kan_Li 

Thanks. I have already converted tflite to tflite .C array. I need to guide to evaluate .tflite .C array on PC. In general, we directly deploy .tflite C array on board without performance validation. Because I could not find any guide to do this, so I opened this topic.

0 项奖励
回复