Among the default value of interrupt priority for the peripherals, which peripheral would have higher priority?
i.e. Non of the peripheral are configured for Interrupt priority, then in that case all are of high priority "0" then how is the priority among peripherals?