Interrupt Priority in LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt Priority in LPC546xx

2,064 Views
hemanthvasista
Contributor IV

Hello ,

I am using the LPC54628 (OM13098).

What is the default value of interrupt priority of ADC, I2C, PINT, CAN, etc.. if not set to any value?


regards,
Hemanth

Labels (1)
0 Kudos
Reply
3 Replies

2,011 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hemanth,

The default value of interrupt priority of ADC, I2C, PINT, CAN is 0, where 0 is the highest priority.

Regards,

Alice

0 Kudos
Reply

2,011 Views
hemanthvasista
Contributor IV

Hello Alice,

Among the default value of interrupt priority for the peripherals, which peripheral would have higher priority?

i.e. Non of the peripheral are configured for Interrupt priority, then in that case all are of high priority "0" then how is the priority among peripherals?

regards,

Hemanth

0 Kudos
Reply

2,011 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hemanth,

"which peripheral would have higher priority?", same priority, system will priority run the interrupt

that first Interrupted.

About the detail interrupt, recommend you have a look at <ARM Cortex-M4 Processor Technical Reference Manual>at ARM website: 

https://developer.arm.com/documentation/100166/0001 

Regards,

Alice

0 Kudos
Reply