Inquiry about Matter commissioning failure with FRDM-RW612 and chip-tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiry about Matter commissioning failure with FRDM-RW612 and chip-tool

119件の閲覧回数
Nokhysh
Contributor I

Dear NXP Support,

I am currently testing Matter with the FRDM-RW612 board and NXP Matter SDK. However, I encountered an issue where commissioning fails when using chip-tool.

Environment

  • Hardware: FRDM-RW612, USB Type-C cable, Windows 11 (64bit) PC

  • Software:

    • WSL2 (Ubuntu 22.04.5 LTS)

    • SEGGER J-Link (Windows, Linux)

    • Matter source: project-chip/connectedhomeip (latest release)

  • Build:

    • Built examples/all-clusters-app/nxp/rt/rw61x with chip_enable_wifi=true

    • Programmed the board via JLink + GDB

Steps performed

  • Flashed FRDM-RW612 successfully and confirmed it boots

  • Executed chip-tool pairing ble-wifi <node_id> <SSID> <PASS> <pin_code> <discriminator>

Issue

  • The commissioning fails with the following error:

 
src/platform/Linux/BLEManagerImpl.cpp:695: Ble Error 0x00000401: BLE adapter unavailable
  • Running bluetoothctl also shows that Bluetooth is not available inside WSL2.

Questions

  1. Is it correct that commissioning with chip-tool is not possible under WSL2 because BLE is not available?

  2. If I switch to a native Linux (Ubuntu) environment instead of WSL2, will it be possible to use chip-tool with BLE commissioning from the PC?

I would greatly appreciate your confirmation and guidance on this matter.

Best regards,
Naoki Hayashi

0 件の賞賛
返信
1 返信

11件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Nokhysh 

I will check and reply to you ASAP.

 

Best regards,

Christine.

0 件の賞賛
返信