If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

Jump to solution
372 Views
chengsz12060
Contributor II

My board is MCU S32K144.
I need to use two channels CAN.
CAN0→CAN-FD
CAN1→CAN Classical
CAN2→not used

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

Tags (1)
0 Kudos
Reply
1 Solution
350 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@chengsz12060

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

yes,

 

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

CAN1,CAN2 can still enable RX FIFO,

 

View solution in original post

0 Kudos
Reply
1 Reply
351 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@chengsz12060

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

yes,

 

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

CAN1,CAN2 can still enable RX FIFO,

 

0 Kudos
Reply