If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

ソリューションへジャンプ
337件の閲覧回数
chengsz12060
Contributor II

My board is MCU S32K144.
I need to use two channels CAN.
CAN0→CAN-FD
CAN1→CAN Classical
CAN2→not used

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

タグ(1)
0 件の賞賛
返信
1 解決策
315件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@chengsz12060

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

yes,

 

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

CAN1,CAN2 can still enable RX FIFO,

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
316件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@chengsz12060

Question1:
Is it allowed to use CAN1's Rx FIFO when CAN1 (CAN Classical) receives data?

yes,

 

Question2:
If CAN0 FD is enabled, are all CAN channels not allowed to use Rx FIFO?

CAN1,CAN2 can still enable RX FIFO,

 

0 件の賞賛
返信