I2C slave EDMA transfer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C slave EDMA transfer

1,613 次查看
k82f_newbie
Contributor I

On the MK82FN256VLL15, Is it possible to use I2C Slave with EDMA? If so, is there any example for it?

In the SDK, the example under driver_examples\i2c\edma_b2b_transfer\slave don't seem to be using EDMA.

0 项奖励
回复
3 回复数

1,583 次查看
k82f_newbie
Contributor I

Understood that it is not common, but is it possible, and is there corresponding sample code?

0 项奖励
回复

1,567 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Sorry, we do not have the code.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,603 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

In common, the salve does not use EDMA. It should react the master quickly.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复