How to dowload the SDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to dowload the SDK?

5,255件の閲覧回数
tusoritibor
Contributor II

Hi, I would like to download the SDK, but the download button on the website: "http://www.nxp.com/products/software-and-tools/run-time-software/mcuxpresso-software-and-tools/mcuxp..." doesn't work. (Empty site comes up with only the menu header). I have tried it from 3 browsers, but the result is the same. Does anybody else have the same problem?

タグ(1)
4 返答(返信)

4,797件の閲覧回数
jimcox
Contributor I

I just ran into the same issue.  It's been over a month since the OP reported it and the download web page is the same empty page that was described.

0 件の賞賛
返信

4,797件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

HI Jim,

Issue has been reported and IT is working on the fix as soon as posible can you use the button called "Build your SDK" or try this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

Regards,

0 件の賞賛
返信

4,797件の閲覧回数
benoitverdin
Contributor II

Hi jorge,

SDK download page is still offline and your link "https://mcuxpresso.nxp.com/en/welcome " is also broken... any news from the ITs?

regards

0 件の賞賛
返信

4,797件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hello,

to get MCUXpresso SDK, please use the "Build your SDK" button on the page, or go directly to http://mcuxpresso.nxp.com. Here you can create and download SDK packages using the SDK builder which is the default way how to get MCUXpresso SDKs.

I notified our web team about the empty Download page, sorry for the inconvenience. 

Regards,

Lukas

0 件の賞賛
返信