Hi
Jlink to has 20pin interface which can not connect OM40006 board.
You need use a Jtag 20 pin to SWD 10 pin adapter/converter to adapt them.
Actually, OM40006 J7 interface can be used to debug the LPC54018 well. I suggest you using it as debug interface.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------