How to connect J-Link to OM40006

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect J-Link to OM40006

948 次查看
sun_xinrui
Contributor I

Hi,

I found OM4006(LPC54018) has a non-standard SWD interface. I can't connect J-Link to OM4006.

J-Link has a 20 pin interface, OM40006 has a 10 pin mini interface. 

Do you have any suggestion about how to connect it? Or do you know how to by an adapter about it?

Thanks,

0 项奖励
回复
1 回复

882 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

Jlink to has 20pin interface which can not connect OM40006 board.

You need use a Jtag 20 pin to  SWD 10 pin adapter/converter to adapt them.

Actually, OM40006 J7 interface can be used to debug the LPC54018 well. I suggest you using it as debug interface.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复