GPIO Slew Rate for KL03

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Slew Rate for KL03

Jump to solution
1,050 Views
McLuhan
Contributor II

Hello,

I'm trying to setup my first project with MCUXpresso with MKL03Z4 SDK.

Using the pin configuration I found that some ports, configured as digital output, have a slow slew rate as default, other ones have a fast slew rate.

GPIO slew rate.png

There's a way to align the slew rate for all the outputs?

In the manual of the MCU I found these specs:

slew rate 2.png

It could be a solution to set the slew rate to "no init" to all the outputs? 

I thank you for your help!

MC

 

Tags (1)
0 Kudos
1 Solution
1,036 Views
ErichStyger
Senior Contributor V

It really depends on the device, and on the pins. To my knowledge you can change or affect the slew range for some pins, but not for all.

View solution in original post

0 Kudos
3 Replies
1,046 Views
ErichStyger
Senior Contributor V

'no init' simply means that it does not get changed/initialized after reset, so it keeps the setting out of reset.

Tags (1)
0 Kudos
1,043 Views
McLuhan
Contributor II

Thank you ErichS.

So it seems that the slew rate is a factory setting that it is not possible to be changed.

0 Kudos
1,037 Views
ErichStyger
Senior Contributor V

It really depends on the device, and on the pins. To my knowledge you can change or affect the slew range for some pins, but not for all.

0 Kudos