FlexSPI Parallel Mode 2 QSPI flashes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FlexSPI Parallel Mode 2 QSPI flashes

跳至解决方案
3,123 次查看
Dave_Cogley
Contributor I

Hello,

I have a question regarding using FlexSPI in parallel mode. I have 2 identical 8MB flashes (Winbond W25Q64JV) hooked up using QSPI on Port A1 and Port B1. The question is, does this make both flashes addressable? Meaning Port A1 is address range 6000_0000 ~ 6080_0000 and Port B1 is 6080_0000 ~ 6100_0000? When do I set bit 31 on register IPCR1? Does it need to be set before every every transfer, or is setup beforehand? In parallel mode, are both chip selects used?

It is important to note, Port A1 is running XIP and Port B1 is used as a data flash.

Dave

0 项奖励
回复
1 解答
3,087 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
According to your schematic and purpose, it should use the individual mode device connection to connect the two QSPI flashes (W25Q64JV), the FlexSPI1 Parallel Mode Device Connection is not suitable.

jeremyzhou_0-1661752056052.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,112 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @Dave_Cogley ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I think I'd like to know more information, so whether you can share the schematic of the FlexSPI connection.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,102 次查看
Dave_Cogley
Contributor I

Sorry for the delay. As you can see U12 is the XIP flash and U17 is the DATA flash.

0 项奖励
回复
3,088 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
According to your schematic and purpose, it should use the individual mode device connection to connect the two QSPI flashes (W25Q64JV), the FlexSPI1 Parallel Mode Device Connection is not suitable.

jeremyzhou_0-1661752056052.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复