Hi,
is there any FreeRTOS driver available for FlexCAN? The SDK currently includes FreeRTOS drivers for SPI, I2C and UART. Any reason there is none available for FlexCAN?
Regards
Markus
解決済! 解決策の投稿を見る。
Hi Markus:
There is no special reason for no flexCAN freeRTOS driver. I will issue a new feature request to the develop team.
The FreeRTOS driver is a wrapper built on top of standard SDK peripheral drivers.
The wrappers provide an API which blocks the calling task until the I/O operation completes and allows other tasks to run. This is achieved by using the asynchronous API of the underlying driver along with RTOS task synchronization object.
You can refer to the FreeRTOS usart driver in SDK installation folder. I am assuming you are using K64.
SDK_2.5.0_TWR-K64F120M\devices\MK64F12\drivers\fsk_uart_freertos.c
SDK_2.5.0_TWR-K64F120M\devices\MK64F12\drivers\fsk_uart_freertos.h
Regards
Daniel
Hi Markus:
There is no special reason for no flexCAN freeRTOS driver. I will issue a new feature request to the develop team.
The FreeRTOS driver is a wrapper built on top of standard SDK peripheral drivers.
The wrappers provide an API which blocks the calling task until the I/O operation completes and allows other tasks to run. This is achieved by using the asynchronous API of the underlying driver along with RTOS task synchronization object.
You can refer to the FreeRTOS usart driver in SDK installation folder. I am assuming you are using K64.
SDK_2.5.0_TWR-K64F120M\devices\MK64F12\drivers\fsk_uart_freertos.c
SDK_2.5.0_TWR-K64F120M\devices\MK64F12\drivers\fsk_uart_freertos.h
Regards
Daniel
4 years later, has this gotten implemented? I don't see it available in MCUXpresso SDK 2.13.0
Hi Daniel,
thanks four your answer. The UART FreeRTOS drivers helped me a lot to develop my own FlexCAN FreeRTOS driver.
Hi @buettgenbach, I also need to write a FlexCAN FreeRTOS driver and was hoping you would be able to share/post the one you created?