Eclipse Marketplace Client

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Eclipse Marketplace Client

跳至解决方案
5,010 次查看
driesmoors
NXP Employee
NXP Employee

Hi,

How can I install the Eclipse Marketplace Client in MCUXpresso? It is not available by default under Help > Install new software... 

After adding the repository http://download.eclipse.org/mpc/neon, I can select the plugin, but installation cannot be completed due to a missing requirement:

Cannot complete the install because one or more required items could not be found.
Software being installed: Marketplace Client 1.5.1.v20160929-1432 (org.eclipse.epp.mpc.feature.group 1.5.1.v20160929-1432)
Missing requirement: Marketplace Client 1.5.1.v20160929-1432 (org.eclipse.epp.mpc.feature.group 1.5.1.v20160929-1432) requires 'org.eclipse.equinox.p2.discovery.feature.feature.group [1.0.0.v201004,2.0.0)' but it could not be found

What other repositories need to be added, and which plugins need to be minimally installed?

Thanks,
Dries.

标签 (1)
标记 (1)
1 解答
3,113 次查看
scaggsp
Contributor II

Try installing from the releases repository.

http://download.eclipse.org/releases/neon

The Eclipse Marketplace Client is under General Purpose Tools → Marketplace Client

在原帖中查看解决方案

2 回复数
3,114 次查看
scaggsp
Contributor II

Try installing from the releases repository.

http://download.eclipse.org/releases/neon

The Eclipse Marketplace Client is under General Purpose Tools → Marketplace Client

3,114 次查看
driesmoors
NXP Employee
NXP Employee

Thanks, that worked.

Any reason why the Neon release repo is not included by default? And why the Marketplace is not installed by default?