Does the TCP/IP stack included with the SDK for the K82 support IPV6 FreeRTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the TCP/IP stack included with the SDK for the K82 support IPV6 FreeRTOS?

1,216件の閲覧回数
lornajones
Contributor I

Does the TCP/IP stack included with the SDK for the K82 support IPV6 FreeRTOS?

0 件の賞賛
返信
1 返信

1,022件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lorna Jones,

The K82 SDK doesn't come with lwIP TCP/IP stack. It is only available for the following devices:

pastedImage_1.png

The lwIP stack does support IPv6. It can be enabled by defining the macro LWIP_IPV6 to 1.

Regards,

Gerardo

0 件の賞賛
返信