Corrupted SDK archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Corrupted SDK archive

1,593 Views
brianzenowich
Contributor I

Build Date: 2018-06-18, Device: MK64FN1M0xxx12

OS: Linux, Toolchain: GCC ARM Embedded

Components: CMSIS DSP Library

SDK Version: KSDK 2.4.0 (2018-06-05)

The zip archive is always corrupt, no matter what components I choose. Please help!

3 Replies

1,456 Views
PetrKraus
NXP Employee
NXP Employee

Hi,

the problem is in the ZIP file name extension. That is incorrectly added to the packages generated for Linux or Mac OS. Please, change it to tar.gz and proceed with decompressing.

This problem will be fixed on the website early next week.

We are sorry for the inconvenience.

1,456 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi  Brian

I would suggest you select all components and all tool chains before downloading, then check whether it is OK or not. 

I tried this on my side, it is OK.

Regards

Daniel

0 Kudos
Reply

1,456 Views
brianzenowich
Contributor I

Hello,

Neither the Windows 10 unzip tool nor the Ubuntu Linux archive manager

could open the zip file, but 7-Zip for Windows was able to recover a

single large tar file from the zip. After un-tarring, all the SDK files

were there!

You might want to take a look at your SDK builder, though. It is

frustrating that it is creating corrupted zip files that are not

accessible from the default unzip apps on both Windows and Linux!

Thanks,

0 Kudos
Reply