Correct SDK for MK22FN256CAP12 microcontroller project creation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Correct SDK for MK22FN256CAP12 microcontroller project creation

1,130 次查看
BR95
Contributor I

Hello! 

I need to create a project for MK22FN256CAP12 microcontroller. I'm using MCUXpresso v11.1.1, and have downloaded SDK_2_4_1_MK22FN256xxx12. However, when i'm creating a project using these sdk version, this microcontroller option does not appear in the Device Package field. What is the correct SDK for MK22FN256CAP12 microcontroller? 

Best regards, 

Bruno.

 

 

 

0 项奖励
回复
2 回复数

1,118 次查看
BR95
Contributor I

Thank you very much, Robin! 

0 项奖励
回复

1,125 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bruno,

Please download the SDK_2.12.0_MK22FN512xxx12.
Select MK22FN512CAP12 when chose Device Packages, manually change the size of Flash to 0x40000.

Device Packages MK22FN256CAP12.pngMemory Configuration.pngFlash Memory Sizes.pngSRAM sizes.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------