Complete FlexSPI Configuration with ROM_FLEXSPI_NORFlash_Init

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Complete FlexSPI Configuration with ROM_FLEXSPI_NORFlash_Init

跳至解决方案
679 次查看
mastupristi
Senior Contributor I

Hi everyone,

I’m using the ROM API function ROM_FLEXSPI_NORFlash_Init() to initialize my QSPI NOR flash, and I pass in a pointer to a flexspi_nor_config_t instance built from these underlying structures:

/*! @brief FLEXSPI Memory Configuration Block */
typedef struct _flexspi_mem_config
{
    uint32_t tag;       /*!< [0x000-0x003] Tag, fixed value 0x42464346UL */
    uint32_t version;   /*!< [0x004-0x007] Version,[31:24] -'V', [23:16] - Major, [15:8] - Minor, [7:0] - bugfix */
    uint32_t reserved0; /*!< [0x008-0x00b] Reserved for future use */
    uint8_t readSampleClkSrc;    /*!< [0x00c-0x00c] Read Sample Clock Source, valid value: 0/1/3 */
    uint8_t csHoldTime;          /*!< [0x00d-0x00d] Data hold time, default value: 3 */
    uint8_t csSetupTime;         /*!< [0x00e-0x00e] Date setup time, default value: 3 */
    uint8_t columnAddressWidth;  /*!< [0x00f-0x00f] Column Address with, for HyperBus protocol, it is fixed to 3, For
                                                    Serial NAND, need to refer to datasheet */
    uint8_t deviceModeCfgEnable; /*!< [0x010-0x010] Device Mode Configure enable flag, 1 - Enable, 0 - Disable */
    uint8_t deviceModeType; /*!< [0x011-0x011] Specify the configuration command type:Quad Enable, DPI/QPI/OPI switch,
                                               Generic configuration, etc. */
    uint16_t waitTimeCfgCommands;    /*!< [0x012-0x013] Wait time for all configuration commands, unit: 100us, Used for
                                                        DPI/QPI/OPI switch or reset command */
    flexspi_lut_seq_t deviceModeSeq; /*!< [0x014-0x017] Device mode sequence info, [7:0] - LUT sequence id, [15:8] - LUt
                                                        sequence number, [31:16] Reserved */
    uint32_t deviceModeArg;          /*!< [0x018-0x01b] Argument/Parameter for device configuration */
    uint8_t configCmdEnable;         /*!< [0x01c-0x01c] Configure command Enable Flag, 1 - Enable, 0 - Disable */
    uint8_t configModeType[3];       /*!< [0x01d-0x01f] Configure Mode Type, similar as deviceModeTpe */
    flexspi_lut_seq_t
        configCmdSeqs[3]; /*!< [0x020-0x02b] Sequence info for Device Configuration command, similar as deviceModeSeq */
    uint32_t reserved1;   /*!< [0x02c-0x02f] Reserved for future use */
    uint32_t configCmdArgs[3];     /*!< [0x030-0x03b] Arguments/Parameters for device Configuration commands */
    uint32_t reserved2;            /*!< [0x03c-0x03f] Reserved for future use */
    uint32_t controllerMiscOption; /*!< [0x040-0x043] Controller Misc Options, see Misc feature bit definitions for more
                                      details */
    uint8_t deviceType;            /*!< [0x044-0x044] Device Type:  See Flash Type Definition for more details */
    uint8_t sflashPadType; /*!< [0x045-0x045] Serial Flash Pad Type: 1 - Single, 2 - Dual, 4 - Quad, 8 - Octal */
    uint8_t serialClkFreq; /*!< [0x046-0x046] Serial Flash Frequencey, device specific definitions, See System Boot
                                              Chapter for more details */
    uint8_t
        lutCustomSeqEnable; /*!< [0x047-0x047] LUT customization Enable, it is required if the program/erase cannot
                                              be done using 1 LUT sequence, currently, only applicable to HyperFLASH */
    uint32_t reserved3[2];  /*!< [0x048-0x04f] Reserved for future use */
    uint32_t sflashA1Size;  /*!< [0x050-0x053] Size of Flash connected to A1 */
    uint32_t sflashA2Size;  /*!< [0x054-0x057] Size of Flash connected to A2 */
    uint32_t sflashB1Size;  /*!< [0x058-0x05b] Size of Flash connected to B1 */
    uint32_t sflashB2Size;  /*!< [0x05c-0x05f] Size of Flash connected to B2 */
    uint32_t csPadSettingOverride;       /*!< [0x060-0x063] CS pad setting override value */
    uint32_t sclkPadSettingOverride;     /*!< [0x064-0x067] SCK pad setting override value */
    uint32_t dataPadSettingOverride;     /*!< [0x068-0x06b] data pad setting override value */
    uint32_t dqsPadSettingOverride;      /*!< [0x06c-0x06f] DQS pad setting override value */
    uint32_t timeoutInMs;                /*!< [0x070-0x073] Timeout threshold for read status command */
    uint32_t commandInterval;            /*!< [0x074-0x077] CS deselect interval between two commands */
    flexspi_dll_time_t dataValidTime[2]; /*!< [0x078-0x07b] CLK edge to data valid time for PORT A and PORT B */
    uint16_t busyOffset;                 /*!< [0x07c-0x07d] Busy offset, valid value: 0-31 */
    uint16_t busyBitPolarity; /*!< [0x07e-0x07f] Busy flag polarity, 0 - busy flag is 1 when flash device is busy, 1 -
                                                 busy flag is 0 when flash device is busy */
    uint32_t lookupTable[64]; /*!< [0x080-0x17f] Lookup table holds Flash command sequences */
    flexspi_lut_seq_t lutCustomSeq[12]; /*!< [0x180-0x1af] Customizable LUT Sequences */
    uint32_t reserved4[4];              /*!< [0x1b0-0x1bf] Reserved for future use */
} flexspi_mem_config_t;

/*! @brief  Serial NOR configuration block */
typedef struct _flexspi_nor_config
{
    flexspi_mem_config_t memConfig; /*!< Common memory configuration info via FLEXSPI */
    uint32_t pageSize;              /*!< Page size of Serial NOR */
    uint32_t sectorSize;            /*!< Sector size of Serial NOR */
    uint8_t ipcmdSerialClkFreq;     /*!< Clock frequency for IP command */
    uint8_t isUniformBlockSize;     /*!< Sector/Block size is the same */
    uint8_t isDataOrderSwapped;     /*!< Data order (D0, D1, D2, D3) is swapped (D1,D0, D3, D2) */
    uint8_t reserved0[1];           /*!< Reserved for future use */
    uint8_t serialNorType;          /*!< Serial NOR Flash type: 0/1/2/3 */
    uint8_t needExitNoCmdMode;      /*!< Need to exit NoCmd mode before other IP command */
    uint8_t halfClkForNonReadCmd;   /*!< Half the Serial Clock for non-read command: true/false */
    uint8_t needRestoreNoCmdMode;   /*!< Need to Restore NoCmd mode after IP commmand execution */
    uint32_t blockSize;             /*!< Block size */
    uint32_t reserve2[11];          /*!< Reserved for future use */
} flexspi_nor_config_t;

 

Recently I learned that at least the LUT isn’t automatically written into the hardware when you call the ROM init function (see https://community.nxp.com/t5/MCUXpresso-SDK/Getting-SFDP-parameters-from-QSPI-NOR-flash-using-ROMAPI...). As a result, everything works only after I manually update the LUT in the peripheral.

Could you please clarify:

  1. Which additional steps must I perform by hand before or after calling ROM_FLEXSPI_NORFlash_Init()?
  2. Do I need to configure the FlexSPI controller registers myself—even though the flexspi_nor_config_t provides all the necessary fields for this?
  3. Are there other configuration commands or ROM API calls that should be executed to apply all of the settings in flexspi_nor_config_t?
  4. What should the field configure or communicate to the driver flexspi_nor_config.ipcmdSerialClkFreq?

best regards

Max

标记 (3)
0 项奖励
回复
1 解答
637 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

After confirming with the internal team that this is a ROM limitation, the `ROM_FLEXSPI_NORFlash_Init` in the ROM API will only recognize and enable a few fixed location LUTs, including read\write\erase.

Therefore, it is recommended to use `ROM_FLEXSPI_NorFlash_UpdateLut` for any other user-added commands in this ROMAPI project.

Best regards,
Gavin

在原帖中查看解决方案

0 项奖励
回复
2 回复数
646 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

Thanks for open this new thread!

The issue is ROM related and I am checking with the internal team. I will sync with you once I get new developments. Please give me some time and thanks in advance!

Best regards,
Gavin

0 项奖励
回复
638 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mastupristi ,

After confirming with the internal team that this is a ROM limitation, the `ROM_FLEXSPI_NORFlash_Init` in the ROM API will only recognize and enable a few fixed location LUTs, including read\write\erase.

Therefore, it is recommended to use `ROM_FLEXSPI_NorFlash_UpdateLut` for any other user-added commands in this ROMAPI project.

Best regards,
Gavin

0 项奖励
回复