Can I use the MIMXRT1050-EVKB SDK for the board MIMXRT1050-EVK ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the MIMXRT1050-EVKB SDK for the board MIMXRT1050-EVK ?

Jump to solution
1,205 Views
wassimhammami
Contributor II

Hi,

I have a MIMXRT1050-EVK (not EVKB) and when I want to download the SDK for the EVK, I found that it is not recommanded (As indicated in the picture I attached).

So my question is : since the MIMXRT1050-EVK SDK is not recommanded, Can I use the MIMXRT1050-EVKB SDK for the board MIMXRT1050-EVK ? Will I have problems

I am inteding to make project using UART communication between two boards (STM32F7 and MIMXRT boards)

Thanks,

Wassim Hammami

mimxrt1050-evk‌ evk-mimxrt1050‌ mimxrt1050-evkb‌ #mcuxpresso sdk

0 Kudos
Reply
1 Solution
1,042 Views
BlackNight
NXP Employee
NXP Employee

Hi Wassim,

I'm using the SDK for the EVKB for both the EVK and EVKB board, and for me things are much better with the EVKB SDK version, see as well i.MX RT1050 EVK vs. EVKB | MCU on Eclipse .

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
1,043 Views
BlackNight
NXP Employee
NXP Employee

Hi Wassim,

I'm using the SDK for the EVKB for both the EVK and EVKB board, and for me things are much better with the EVKB SDK version, see as well i.MX RT1050 EVK vs. EVKB | MCU on Eclipse .

I hope this helps,

Erich

0 Kudos
Reply
1,042 Views
wassimhammami
Contributor II

Hi Erich,

Thanks for the info, I will use the SDK of EVKB for the EVK. I don't think there will be a problem

Happy coding ! 

Wassim

0 Kudos
Reply