Can I re-distribute the USB CDC driver included MCUXpressoSDK?

cancel
Showing results for 
Search instead for 
Did you mean: 

Can I re-distribute the USB CDC driver included MCUXpressoSDK?

Jump to solution
350 Views
masahirokiniwa
Contributor IV

I will use USB CDC based on MCUXpressoSDK with Kinetis K27.
Can I re-distribute its driver which NXP provided with usb_examples?

If I must check the license agreement for using and re-distributing it, could you tell me it?

Best regards,
M.Kiniwa

0 Kudos
1 Solution
181 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Masahiro Kiniwa 

When you download the software package and you agree on the Software Terms and Conditions, you accept the USB drivers with license: Open Source - BSD-3-Clause Clear. I recommend you to read the license agreement for more information.

Hope this information helps.

Best regards

Jorge Alcala

View solution in original post

0 Kudos
2 Replies
182 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Masahiro Kiniwa 

When you download the software package and you agree on the Software Terms and Conditions, you accept the USB drivers with license: Open Source - BSD-3-Clause Clear. I recommend you to read the license agreement for more information.

Hope this information helps.

Best regards

Jorge Alcala

View solution in original post

0 Kudos
181 Views
masahirokiniwa
Contributor IV

Hi Jorge,

Thank you for your answer.

I see that the CDC driver is included the software terms of the software package.

I confirmed it for use SDK, so I will consider the availability of CDC driver under the software terms.

Best regards,

M.Kiniwa

0 Kudos