CMISI interrupt priority

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMISI interrupt priority

1,488件の閲覧回数
tobias_mrs
Contributor III

Hello I work on a Kinetis MKE18F512 with SDK 2.6 and  now I have problems to understand and use the interrupts in a correct way.
My Problem:

I have interrupt settings at reset state.
I drive a system-timer wit the sysTick interrupt. Now if I use a UART transfer the sysTick don't run and I don't get any timings.
It also don't help to lower the UART interrupt priority by

   NVIC_SetPriority( LPUART0_TX_IRQn, 1 );
   NVIC_SetPriority( LPUART0_RX_IRQn, 1 );
   NVIC_SetPriority( CAN0_ORed_IRQn, 2 );
   NVIC_SetPriority( CAN0_Error_IRQn, 2 );
   NVIC_SetPriority( CAN0_Wake_Up_IRQn, 2 );
   NVIC_SetPriority( CAN0_ORed_Message_buffer_IRQn, 2 );

If one interrupt is running no other will be called.
How could I setup that the systick interrupt can preempt all others?

0 件の賞賛
返信
2 返答(返信)

1,376件の閲覧回数
tobias_mrs
Contributor III

I have found the problem:

The function SysTick_Config(uint32_t ticks) set the interrupt priority of the sysTick to 15. That means the lowest priority.

The solution was to reset the priority after calling the init function

    if( 0 != SysTick_Config( SystemCoreClock / 1000 ) )
    {
        ret = HAL_ERR_INIT;
    }
    else
    {
        NVIC_SetPriority( SysTick_IRQn, 0 );
        // no errors
    }  


Bu for further information's.
Could you lead me to a example how to configure the interrupt priority with the SDK.

0 件の賞賛
返信

1,376件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi Tobias,

 

I am very happy that the problem has been resolved. Unfortunately, there are no examples with that specific functionality that show the use of NVIC.

 

If you have any questions please don't hesitate to ask.

 

Best Regards,

Ricardo

0 件の賞賛
返信