Build Errors on JN-AN-1174, the IEEE 802.15.4 App for JN516x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Errors on JN-AN-1174, the IEEE 802.15.4 App for JN516x

1,760件の閲覧回数
mferrari1
Contributor III

I just installed "BeyondStudio for NXP", then installed the "JN516x IEEE 802.15.4 SDK", then imported the JN-AN-1174 project, but when I build it, I get tons of errors because of unresolved definitions.  Are there additional entities that need to be imported into the Workspace in order to successfully build this project?  Are there special path specifications required?  I've followed all the instructions for the SDK and the JN-AN-1174.  I expected it to build...  Any help is appreciated - thanks!  (Screenshot included).

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,566件の閲覧回数
mferrari1
Contributor III

I cleared the errors and rebuit and now it seems to build OK and reports no errors.  Not sure why the errors appeared initially.  Any ideas about that?  It seems to be building without errors now...

0 件の賞賛
返信

1,566件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Matt,

Could you please look at the next community document?

Beyond Studio Common Errors

Please let me know if you have further questions.

Regards,

Mario

0 件の賞賛
返信