Bug in fsl_clock.c in SDK for LPC812

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in fsl_clock.c in SDK for LPC812

944 Views
petrolivka
Contributor II

Hi!

  The frequency of USART is not correctly computed in file fsl_clock.c in SDK 2.9.0 for LPC812. 

  The current code is:

uint32_t CLOCK_GetUartClkFreq(void)
{
    uint32_t freq = CLOCK_GetMainClkFreq();
    uint32_t uartDiv = SYSCON->UARTCLKDIV & 0xffU;

    return uartDiv == 0U ? 0U :
    (uint32_t)((uint64_t)(freq << 8U) /
        (uartDiv * (256U + ((SYSCON->UARTFRGMULT) & SYSCON_UARTFRGMULT_MULT_MASK))));
}

The variable freq should be retyped to uint64_t before shift left. Better is:

return uartDiv == 0U ? 0U : (uint32_t)((((uint64_t)(freq)) << 8U) /....

It is easy to test it for MainClock 24 MHz, UARTCLKDIV =1 and UARTFRGMULT=0. The correct result should be 24 MHz, but the function returns bad result: 7222784 Hz. 

The 24 MHz is 0x16E3600 and after shift left is out of range of uint32_t. 

Petr

 

 

 

1 Reply

929 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi petrolivka

We will fix this problem in release SDK2.11.0.

Thank you for bringing the problem to our attention.

 

Best Regards

Jun Zhang

0 Kudos
Reply