I'm having problems with MCUXpresso IDE. I'm trying to generate an SDK for the K64FN using the Install New Plugin SDK button found on the Installed SDKs view. But after finishing generating the project I have this malformed SDK:
I can see on my /usr/local/mcuxpressoide-11.2.1_4149/ide/plugins path the following:
As you can see, there is my correctly generated SDK for the MK10DN processor and a weird .zip file for the MK64FN.
Does anyone know what's going on?
_______________________________________________
EDIT:
I tried uninstalling the SDKs and deleting the folders manually to start from scratch. I was able to create the SDK fir the K10FN without any problems. But when trying to create the one for the K64FN I get this:
Solved! Go to Solution.
@danielchen did you try to reproduce using MCUXpresso 11.2.1? I think this is happening because as explained in another question I posted, the IDE is trying to get the newest version of the SDK and the 2.9.0 is not compatible with MCUXpresso 11.2.1.
I have downloaded 11.3.0 and the problem doesn't manifest in it, so I guess this is not a problem anymore.
Hi
I can not reproduce your issue on my side. Please see my below picture, I can find the right SDK with key word 'k64fn '.
MCUXpresso IDE 11.3.0 is released . You can download this version from below link.
Regards
Daniel
@danielchen did you try to reproduce using MCUXpresso 11.2.1? I think this is happening because as explained in another question I posted, the IDE is trying to get the newest version of the SDK and the 2.9.0 is not compatible with MCUXpresso 11.2.1.
I have downloaded 11.3.0 and the problem doesn't manifest in it, so I guess this is not a problem anymore.
I didn't try that with MCUXpresso IDE 11.2.1, I have updated IDE to 11.3.0 before you reported it. Glad to hear that it is not a problem any more
Regards
Daniel