I am using iMXRT1170 EVK with MCU Link Pro as the debugger. The new version of MCUXpresso was even more unreliable than v11.4.1. More or less 50% of the times I start a debug session it fails and I must power cycle both EVK and MCU Link Pro. I am using Ubuntu 18.04:
erling@ubuntu-ntnu ~> uname -a
Linux ubuntu-ntnu 5.4.0-99-generic #112~18.04.1-Ubuntu SMP Thu Feb 3 14:09:57 UTC 2022 x86_64 x86_64 x86_64 GNU/Linux
Hi,
We cannot reproduce locally this problem. It is possible to pack the eclipse log plus console logs and send us to investigate? You can achieve this by using Save Info for Support option which generates a zip file with all the logs:
When choosing this option, all files going to archive will be listed. We recommend to let them all selected as they are set by default.
Regards,
MCUXpresso IDE Support
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
When using the on-board debug tool instead of MCU Link Pro, does the unstable debugging phenomenon also happen?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------