v11.0.1 "Manage SDK Components" removes " from C++ Symbols

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

v11.0.1 "Manage SDK Components" removes " from C++ Symbols

Jump to solution
1,484 Views
wilkinsw
Contributor III

I am using version 11.0.1 of MCUXpresso (Build 2563) with the mbedTLS library middleware.

mbedTLS requires that you define MBEDTLS_CONFIG_FILE with the name of the config header.  This is generated by the SDK to be "ksdk_mbedtls_config.h"

In .cproject this becomes

<listOptionValue builtIn="false" value="MBEDTLS_CONFIG_FILE='&quot;ksdk_mbedtls_config.h&quot;'"/>

If you run "Manage SDK Components" and make any change that updates .cproject the C++ version of this symbol has the &quot removed to become this:

<listOptionValue builtIn="false" value="MBEDTLS_CONFIG_FILE='ksdk_mbedtls_config.h'"/>

Which causes include errors due to no longer being wrapped in quotes.  You then have to open up the properties and add quotes back to the symbol manually.

This only happens with 'GNU C++' language symbols, it does not affect 'GNU C' symbols

0 Kudos
Reply
1 Solution
1,394 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Thanks for the report. We'll investigate.

Regards,

MCUXpresso IDE Support

View solution in original post

0 Kudos
Reply
2 Replies
1,395 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Thanks for the report. We'll investigate.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply
1,394 Views
wilkinsw
Contributor III

As a workaround you can use <> instead of ""

MBEDTLS_CONFIG_FILE '<ksdk_mbedtls_config.h>'

0 Kudos
Reply