uart_interrupt how does DEMO_UART_IRQHandler() get invoked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

uart_interrupt how does DEMO_UART_IRQHandler() get invoked

跳至解决方案
4,013 次查看
stdcerr
Contributor IV

Hi,

 

I have a question regarding uart_interrupt.c:

How does the ISR (DEMO_UART_IRQHandler) get invoked?

I cxhanged the example code from using UART0 to using UART4 and have updated the macros like this:

#define DEMO_UART_IRQn       UART4_RX_TX_IRQn
#define DEMO_UART_IRQHandler UART4_RX_TX_IRQHandler

then enabling the interrupts looks like:

    /* Enable RX interrupt. */
    UART_EnableInterrupts(DEMO_UART, kUART_RxDataRegFullInterruptEnable | kUART_RxOverrunInterruptEnable);
    EnableIRQ(DEMO_UART_IRQn);

but I'm not sure now, if UART4RxInterrupt really invokes DEMO_UART_IRQHandler() and if it does, how is DEMO_UART_IRQHandler associated with the interrupt? I feel like I'm missing a piece somewhere.

0 项奖励
回复
1 解答
3,985 次查看
myke_predko
Senior Contributor III

Hey @stdcerr 

If you Left click on UART4_RX_TX_IRQHandler and then hit F3 (to bring up the definition) you'll see:

WEAK void UART4_RX_TX_IRQHandler(void)
{ UART4_RX_TX_DriverIRQHandler();
}

This is the default definition of the interrupt handler for the UART4 RX/TX and if you repeat the F3 operation with the link inside the method, yoiu'll find that it leads to:

void UART1_RX_TX_DriverIRQHandler(void) ALIAS(IntDefaultHandler);

and if you F3 "IntDefaultHandler" you'll get to:

//*****************************************************************************
// Processor ends up here if an unexpected interrupt occurs or a specific
// handler is not present in the application code.
//*****************************************************************************
WEAK_AV void IntDefaultHandler(void)
{ while(1) {}
}

Which is what you expect (ie if you haven't defined an interrupt handler, you're going to a default one that does nothing).  

The default handler referenced above has the "WEAK" option which means that if the "UART4_RX_TX_IRQHandler" is redefined, as in the definition code, then the original vector (which leads to "IntDefaultHandler") is overwritten with the address of your (or the demo) handler code.  

This is a feature of C99 which is completely non-intuitive but once you understand and accept it things become a bit more consistent when working with things like adding interrupt handlers.  

Good luck,

myke

 

在原帖中查看解决方案

3 回复数
3,986 次查看
myke_predko
Senior Contributor III

Hey @stdcerr 

If you Left click on UART4_RX_TX_IRQHandler and then hit F3 (to bring up the definition) you'll see:

WEAK void UART4_RX_TX_IRQHandler(void)
{ UART4_RX_TX_DriverIRQHandler();
}

This is the default definition of the interrupt handler for the UART4 RX/TX and if you repeat the F3 operation with the link inside the method, yoiu'll find that it leads to:

void UART1_RX_TX_DriverIRQHandler(void) ALIAS(IntDefaultHandler);

and if you F3 "IntDefaultHandler" you'll get to:

//*****************************************************************************
// Processor ends up here if an unexpected interrupt occurs or a specific
// handler is not present in the application code.
//*****************************************************************************
WEAK_AV void IntDefaultHandler(void)
{ while(1) {}
}

Which is what you expect (ie if you haven't defined an interrupt handler, you're going to a default one that does nothing).  

The default handler referenced above has the "WEAK" option which means that if the "UART4_RX_TX_IRQHandler" is redefined, as in the definition code, then the original vector (which leads to "IntDefaultHandler") is overwritten with the address of your (or the demo) handler code.  

This is a feature of C99 which is completely non-intuitive but once you understand and accept it things become a bit more consistent when working with things like adding interrupt handlers.  

Good luck,

myke

 

3,296 次查看
NVazquez
Contributor IV

I'm using spifi driver and sample code of polling transfer. my code was going in  "WEAK_AV void IntDefaultHandler(void)
{ while(1) {}
}"

as well. Why do we need an interrupt handler? Why is the SKD sample code not taking care of the SPIFI interrupt?

0 项奖励
回复
3,994 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi stdcerr:

 

Please see the vector table in devices/MK64F12\mcuxpresso\startup_mk64f12.c,

 

__attribute__ ((used, section(".isr_vector")))
void (* const g_pfnVectors[])(void) = {
// Core Level - CM4
&_vStackTop, // The initial stack pointer
ResetISR, // The reset handler
NMI_Handler, // The NMI handler
HardFault_Handler, // The hard fault handler
MemManage_Handler, // The MPU fault handler
BusFault_Handler, // The bus fault handler
UsageFault_Handler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
SVC_Handler, // SVCall handler
DebugMon_Handler, // Debug monitor handler
0, // Reserved
PendSV_Handler, // The PendSV handler
SysTick_Handler, // The SysTick handler

// Chip Level - MK64F12
DMA0_IRQHandler, // 16 : DMA Channel 0 Transfer Complete
DMA1_IRQHandler, // 17 : DMA Channel 1 Transfer Complete
DMA2_IRQHandler, // 18 : DMA Channel 2 Transfer Complete
DMA3_IRQHandler, // 19 : DMA Channel 3 Transfer Complete
DMA4_IRQHandler, // 20 : DMA Channel 4 Transfer Complete
DMA5_IRQHandler, // 21 : DMA Channel 5 Transfer Complete
DMA6_IRQHandler, // 22 : DMA Channel 6 Transfer Complete
DMA7_IRQHandler, // 23 : DMA Channel 7 Transfer Complete
DMA8_IRQHandler, // 24 : DMA Channel 8 Transfer Complete
DMA9_IRQHandler, // 25 : DMA Channel 9 Transfer Complete
DMA10_IRQHandler, // 26 : DMA Channel 10 Transfer Complete
DMA11_IRQHandler, // 27 : DMA Channel 11 Transfer Complete
DMA12_IRQHandler, // 28 : DMA Channel 12 Transfer Complete
DMA13_IRQHandler, // 29 : DMA Channel 13 Transfer Complete
DMA14_IRQHandler, // 30 : DMA Channel 14 Transfer Complete
DMA15_IRQHandler, // 31 : DMA Channel 15 Transfer Complete
DMA_Error_IRQHandler, // 32 : DMA Error Interrupt
MCM_IRQHandler, // 33 : Normal Interrupt
FTFE_IRQHandler, // 34 : FTFE Command complete interrupt
Read_Collision_IRQHandler, // 35 : Read Collision Interrupt
LVD_LVW_IRQHandler, // 36 : Low Voltage Detect, Low Voltage Warning
LLWU_IRQHandler, // 37 : Low Leakage Wakeup Unit
WDOG_EWM_IRQHandler, // 38 : WDOG Interrupt
RNG_IRQHandler, // 39 : RNG Interrupt
I2C0_IRQHandler, // 40 : I2C0 interrupt
I2C1_IRQHandler, // 41 : I2C1 interrupt
SPI0_IRQHandler, // 42 : SPI0 Interrupt
SPI1_IRQHandler, // 43 : SPI1 Interrupt
I2S0_Tx_IRQHandler, // 44 : I2S0 transmit interrupt
I2S0_Rx_IRQHandler, // 45 : I2S0 receive interrupt
UART0_LON_IRQHandler, // 46 : UART0 LON interrupt
UART0_RX_TX_IRQHandler, // 47 : UART0 Receive/Transmit interrupt
UART0_ERR_IRQHandler, // 48 : UART0 Error interrupt
UART1_RX_TX_IRQHandler, // 49 : UART1 Receive/Transmit interrupt
UART1_ERR_IRQHandler, // 50 : UART1 Error interrupt
UART2_RX_TX_IRQHandler, // 51 : UART2 Receive/Transmit interrupt
UART2_ERR_IRQHandler, // 52 : UART2 Error interrupt
UART3_RX_TX_IRQHandler, // 53 : UART3 Receive/Transmit interrupt
UART3_ERR_IRQHandler, // 54 : UART3 Error interrupt
ADC0_IRQHandler, // 55 : ADC0 interrupt
CMP0_IRQHandler, // 56 : CMP0 interrupt
CMP1_IRQHandler, // 57 : CMP1 interrupt
FTM0_IRQHandler, // 58 : FTM0 fault, overflow and channels interrupt
FTM1_IRQHandler, // 59 : FTM1 fault, overflow and channels interrupt
FTM2_IRQHandler, // 60 : FTM2 fault, overflow and channels interrupt
CMT_IRQHandler, // 61 : CMT interrupt
RTC_IRQHandler, // 62 : RTC interrupt
RTC_Seconds_IRQHandler, // 63 : RTC seconds interrupt
PIT0_IRQHandler, // 64 : PIT timer channel 0 interrupt
PIT1_IRQHandler, // 65 : PIT timer channel 1 interrupt
PIT2_IRQHandler, // 66 : PIT timer channel 2 interrupt
PIT3_IRQHandler, // 67 : PIT timer channel 3 interrupt
PDB0_IRQHandler, // 68 : PDB0 Interrupt
USB0_IRQHandler, // 69 : USB0 interrupt
USBDCD_IRQHandler, // 70 : USBDCD Interrupt
Reserved71_IRQHandler, // 71 : Reserved interrupt
DAC0_IRQHandler, // 72 : DAC0 interrupt
MCG_IRQHandler, // 73 : MCG Interrupt
LPTMR0_IRQHandler, // 74 : LPTimer interrupt
PORTA_IRQHandler, // 75 : Port A interrupt
PORTB_IRQHandler, // 76 : Port B interrupt
PORTC_IRQHandler, // 77 : Port C interrupt
PORTD_IRQHandler, // 78 : Port D interrupt
PORTE_IRQHandler, // 79 : Port E interrupt
SWI_IRQHandler, // 80 : Software interrupt
SPI2_IRQHandler, // 81 : SPI2 Interrupt
UART4_RX_TX_IRQHandler, // 82 : UART4 Receive/Transmit interrupt
UART4_ERR_IRQHandler, // 83 : UART4 Error interrupt
UART5_RX_TX_IRQHandler, // 84 : UART5 Receive/Transmit interrupt
UART5_ERR_IRQHandler, // 85 : UART5 Error interrupt
CMP2_IRQHandler, // 86 : CMP2 interrupt
FTM3_IRQHandler, // 87 : FTM3 fault, overflow and channels interrupt
DAC1_IRQHandler, // 88 : DAC1 interrupt
ADC1_IRQHandler, // 89 : ADC1 interrupt
I2C2_IRQHandler, // 90 : I2C2 interrupt
CAN0_ORed_Message_buffer_IRQHandler, // 91 : CAN0 OR'd message buffers interrupt
CAN0_Bus_Off_IRQHandler, // 92 : CAN0 bus off interrupt
CAN0_Error_IRQHandler, // 93 : CAN0 error interrupt
CAN0_Tx_Warning_IRQHandler, // 94 : CAN0 Tx warning interrupt
CAN0_Rx_Warning_IRQHandler, // 95 : CAN0 Rx warning interrupt
CAN0_Wake_Up_IRQHandler, // 96 : CAN0 wake up interrupt
SDHC_IRQHandler, // 97 : SDHC interrupt
ENET_1588_Timer_IRQHandler, // 98 : Ethernet MAC IEEE 1588 Timer Interrupt
ENET_Transmit_IRQHandler, // 99 : Ethernet MAC Transmit Interrupt
ENET_Receive_IRQHandler, // 100: Ethernet MAC Receive Interrupt
ENET_Error_IRQHandler, // 101: Ethernet MAC Error and miscelaneous Interrupt

}; /* End of g_pfnVectors */

 

when interrupt  (82 : UART4 Receive/Transmit interrupt) fires,  then isr  UART4_RX_TX_IRQHandler will be called.

 

Regards

Daniel