"Please select a target device or a board" shows no options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Please select a target device or a board" shows no options

2,340 Views
injunear
Contributor III

Yesterday I was able to start a new MCUXpresso C project and when I got to the window where I am to select a board to program, MCUXpresso showed me lots of options. Today when I follow the exact same process no boards are shown and I am not able to continue.

To the best of my knowledge, I did not change anything. Where do these board selections come from and why doesn't MCUXpresso show the board options anymore?

Thank you.

0 Kudos
1 Reply

2,006 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hillbilly,

Which chip or board do you used ?

For most of the boards ,  we need first install the SDK package ,

then use the "New project..." button on "Quickstart panel " to create new project.

pastedImage_1.png

About the detail steps please refer to "MCUXpresso_IDE_User_Guide.pdf"->

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos