no live view of global variable in the New 10.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no live view of global variable in the New 10.2.0

Jump to solution
824 Views
haizhouli
Contributor III

I updated the IDE to the newer 10.2.0.

I can debug with the live view of global variable in the older version by using the LPC link 2.  After installing the newer version, the " enable/disable variables update" arrow are always grey, as shown in the picture.  I cannot see any live variables any more. 

Did I miss any setup? 

Thanks a lot!

0 Kudos
1 Solution
729 Views
BlackNight
NXP Employee
NXP Employee

Is your probe running in non-stop-mode?

pastedImage_1.png

Additionally, to turn the 'green arrow' on, your target has to be running (you cannot do this while the target is suspended).

I hope this helps,

Erich

View solution in original post

0 Kudos
2 Replies
729 Views
haizhouli
Contributor III

Hi Erich,

Thanks so much for the reply! I bet the "Non-Stop" is the reason. 

After upgrading, the debug mode still shows "Non-Stop", but the live view does not work. By following your hints, I changed the debug mode to "All-Stop" and then changed it back to "Non-Stop", suddenly, it works!

If anyone else met the same issue, here is the way to fix it.

Thanks again!

Haizhou

0 Kudos
730 Views
BlackNight
NXP Employee
NXP Employee

Is your probe running in non-stop-mode?

pastedImage_1.png

Additionally, to turn the 'green arrow' on, your target has to be running (you cannot do this while the target is suspended).

I hope this helps,

Erich

0 Kudos