mcuxpressoide 11.9.4 Fails to build with unicode characters in user directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcuxpressoide 11.9.4 Fails to build with unicode characters in user directory

420件の閲覧回数
mibli
Contributor II

For Example my user directory is named "Miłosz" and in the build path, it is converted to Milosz, build fails with "C:/User/Milosz/AppData/Local/Temp no such directory."

0 件の賞賛
2 返答(返信)

393件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

It's something that needs some testing/analysis. We'll look into this and get back with conclusions. Not sure about build tools support when it comes to Unicode chars inside paths. Some parts of Eclipse might also not work as expected with such paths.

Meanwhile, please attach support information (Help => MCUXpresso Save Info for Support) after trying to build a project that eventually fails.

Regards,
MCUXpresso IDE Support

394件の閲覧回数
ErichStyger
Senior Contributor V

I think you mean 11.9.0 and not 11.9.4?

Anyway: I'm avoiding non-7-bit-ASCII characters in paths or file names, as it only causes troubles with the GNU toolchain, e.g. include paths and other path or file related things.

What you could use instead on windows: use the 'subst' command to create a virtual drive letter to your projects, e.g.

subst p: C:\User\Milosz\myProjects

and then use the P:\ driver for  it.

0 件の賞賛