mcuxpressoide-11.9.0_2144.x86_64.deb.bin Install Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcuxpressoide-11.9.0_2144.x86_64.deb.bin Install Error

2,965 Views
arunjyothishk
Contributor I

OS: Ubuntu 23.10 x86_64

6.5.0-14-generic

---------------------------------------

╰─○ python3 --version
Python 3.11.6

--------------------------------------

Error while Installing ...

.....
Removing mcuxpressoide (11.9.0) ...
Removing mcuxpressoide symbolic link...
Processing triggers for gnome-menus (3.36.0-1.1ubuntu1) ...
Processing triggers for mailcap (3.70+nmu1ubuntu1) ...
Processing triggers for desktop-file-utils (0.26-1ubuntu5) ...
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
E: Unable to locate package libpython3.8
E: Couldn't find any package by glob 'libpython3.8'


0 Kudos
Reply
2 Replies

2,672 Views
mosesmcknight
Contributor I

I was able to install libpython3.8 on Linuxmint 21.3 (based on Ubuntu 22.04) using the "deadsnakes" ppa.

 
 
 
 
Tags (1)
0 Kudos
Reply

2,944 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Note that Ubuntu 23.10 is not officially supported by MCUXpresso IDE (i.e. we did not explicitly verify it on this OS). Looking at the screenshot you offered, I don't see the full log, so I suggest you manually install "libncursesw5" and "libpython3.8" (the other dependencies are "libusb-1.0-0-dev", "dfu-util" and "libncurses5").

Regards,
MCUXpresso IDE Support

0 Kudos
Reply