mcuxpressoide-11.9.0_2144.x86_64.deb.bin Install Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mcuxpressoide-11.9.0_2144.x86_64.deb.bin Install Error

2,988 次查看
arunjyothishk
Contributor I

OS: Ubuntu 23.10 x86_64

6.5.0-14-generic

---------------------------------------

╰─○ python3 --version
Python 3.11.6

--------------------------------------

Error while Installing ...

.....
Removing mcuxpressoide (11.9.0) ...
Removing mcuxpressoide symbolic link...
Processing triggers for gnome-menus (3.36.0-1.1ubuntu1) ...
Processing triggers for mailcap (3.70+nmu1ubuntu1) ...
Processing triggers for desktop-file-utils (0.26-1ubuntu5) ...
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
E: Unable to locate package libpython3.8
E: Couldn't find any package by glob 'libpython3.8'


0 项奖励
回复
2 回复数

2,695 次查看
mosesmcknight
Contributor I

I was able to install libpython3.8 on Linuxmint 21.3 (based on Ubuntu 22.04) using the "deadsnakes" ppa.

 
 
 
 
标记 (1)
0 项奖励
回复

2,967 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Note that Ubuntu 23.10 is not officially supported by MCUXpresso IDE (i.e. we did not explicitly verify it on this OS). Looking at the screenshot you offered, I don't see the full log, so I suggest you manually install "libncursesw5" and "libpython3.8" (the other dependencies are "libusb-1.0-0-dev", "dfu-util" and "libncurses5").

Regards,
MCUXpresso IDE Support

0 项奖励
回复