mcux sdk components

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcux sdk components

862件の閲覧回数
henning1
Contributor I

Hi

I am working with the k64f freedom board in mcuxpresso with sdk 2.5. In the example code there is this folder called components. I find myself unable to create a new sdk project with these components, and I have also been unsuccessfull in finding the documentation related to their use. (except the docstrings in the headers)

They are not selectable from the list of libraries etc. that is included in the project creation, and the only "components" that is included by default is serial_manager and uart. I would like to play around with the other "components" as well.

Are they supposed to be just drag and dropped from the zip archive into the project folder, or is there a more correct way to use them in a project with the correct defines etc.?

Picture related.

0 件の賞賛
返信
1 返信

753件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Henning:

NXP released SDK_2.6.0_FRDM-K64F. I would suggest you try to download it from below link

https://mcuxpresso.nxp.com/en/select 

and try it again.

Regards

Daniel

0 件の賞賛
返信