http://nxp.com/ksdk/2.0/ksdk_manifest_v3.0.xsd not available (dead link)

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

http://nxp.com/ksdk/2.0/ksdk_manifest_v3.0.xsd not available (dead link)

474件の閲覧回数
dave_carlson
Contributor III

The SDK project files have a reference to "http://nxp.com/ksdk/2.0/ksdk_manifest_v3.0.xsd" but this is a dead link on your website.  Since the sdk references (appear to be) in files generated by the IDE project wizards, this seems to be an IDE issue.

We would like to use the xsd to validate our xml as well as understand the full specification for the project xml. 

It seems odd to use a unavailable xml format for your IDE projects...

dave

0 件の賞賛
1 返信

453件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Dave,

the http://nxp.com/ksdk/2.0/ksdk_manifest_v3.0.xsd  is actually id of a namespace used in manifest file. In order to get XSD, please follow the URL placed as the second argument of xsi:schemaLocation attribute, for example http://nxp.com/mcuxpresso/sdk/sdk_manifest_v3.6.xsd as in xsi:schemaLocation="http://nxp.com/ksdk/2.0/ksdk_manifest_v3.0.xsd http://nxp.com/mcuxpresso/sdk/sdk_manifest_v3.6.xsd".

Regards,

Lukas

0 件の賞賛