gdb serial support for baremetal application ?

cancel
Showing results for 
Search instead for 
Did you mean: 

gdb serial support for baremetal application ?

314 Views
ranshalit
Senior Contributor I

Hello,

Does nxp provide any gdb serial support (for baremetal application) ?

Thanks,

ranran

0 Kudos
3 Replies

201 Views
converse
Senior Contributor V

What do you mean by 'Serial Support'? Are you running a debug monitor on the target? 

Pretty much all debug is done via SWD (built-in debug connection) on Cortex-M parts, or JTAG (old, ARM7 or 9 based parts). The MCUXpresso is NXP's free toolchain (includes GDB and GCC, wrapped in an Eclipse IDE, but you can use them standalone if necessary). If using a SWD/JTAG, you need a debug probe such as LPC-Link2 (about $25), U-Link (Keil), J-Link (Segger) and Mulitlink (PEMicro).

0 Kudos

201 Views
ranshalit
Senior Contributor I

Hi,

I mean that I don't have swd or jtag, only serial.

I know there is something called gdb stub via serial.

But it requires driver/sw support.

Thanks,

ranran

0 Kudos

201 Views
converse
Senior Contributor V

For 'serial' debug, you need a debug monitor running on the target and AFAIK, there is no such thing for any modern ARM-ased MCU's (i.e NXP, ST, etc), So, no, there is no such thing. If you want to debug you *need* SWD. 

For information on how to add SWD, see

https://community.nxp.com/thread/388998 

If this doesn't answer your question, please explain exactly what you have (chip, board ec) and exactly what you are trying to do, and why.

0 Kudos