freeRTOS stack size configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freeRTOS stack size configuration

Jump to solution
4,558 Views
Relas
Contributor I

I am currently learning FreeRTOS on the LPC51U68 development board (OM40005). I have created 7 tasks for testing and am using the RTOS task list monitor provided by MCUXpresso IDE.

I noticed that the stack sizes displayed in the task list don't match the configurations I set.

Could this be related to memory alignment?

Where can I check the rules for configuration differences?

Below is the code I modified from the freertos_hello example.

 

/*

* Copyright (c) 2015, Freescale Semiconductor, Inc.

* Copyright 2016-2017 NXP

* All rights reserved.

*

* SPDX-License-Identifier: BSD-3-Clause

*/

 

/* FreeRTOS kernel includes. */

#include "FreeRTOS.h"

#include "task.h"

#include "queue.h"

#include "timers.h"

 

/* Freescale includes. */

#include "fsl_device_registers.h"

#include "fsl_debug_console.h"

#include "pin_mux.h"

#include "board.h"

 

#include <stdbool.h>

/*******************************************************************************

* Definitions

******************************************************************************/

 

/* Task priorities. */

#define hello_task_PRIORITY (configMAX_PRIORITIES - 1)

/*******************************************************************************

* Prototypes

******************************************************************************/

static void task1(void *pvParameters);

static void task2(void *pvParameters);

static void task3(void *pvParameters);

static void task4(void *pvParameters);

static void task5(void *pvParameters);

static void task6(void *pvParameters);

static void task7(void *pvParameters);

/*******************************************************************************

* Code

******************************************************************************/

/*!

* @brief Application entry point.

*/

int main(void)

{

/* Init board hardware. */

/* attach 12 MHz clock to FLEXCOMM0 (debug console) */

CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

 

BOARD_InitBootPins();

BOARD_InitBootClocks();

BOARD_InitDebugConsole();

if (xTaskCreate(task1, "task1", configMINIMAL_STACK_SIZE + 50, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task2, "task2", configMINIMAL_STACK_SIZE + 100, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task3, "task3", configMINIMAL_STACK_SIZE + 160, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task4, "task4", configMINIMAL_STACK_SIZE + 161, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task5, "task5", configMINIMAL_STACK_SIZE + 170, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task6, "task6", configMINIMAL_STACK_SIZE + 200, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

if (xTaskCreate(task7, "task7", configMINIMAL_STACK_SIZE + 300, NULL, hello_task_PRIORITY, NULL) !=

pdPASS)

{

PRINTF("Task creation failed!.\r\n");

while (1)

;

}

vTaskStartScheduler();

for (;;)

;

}

 

/*!

* @brief Task responsible for printing of "Hello world." message.

*/

static void task1(void *pvParameters)

{

for (;;)

{

PRINTF("Hello world.\r\n");

vTaskSuspend(NULL);

}

}

 

static void task2(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

static void task3(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

static void task4(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

static void task5(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

static void task6(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

static void task7(void *pvParameters)

{

for (;;)

{

PRINTF("H\r\n");

vTaskSuspend(NULL);

}

}

 

Tags (1)
0 Kudos
Reply
1 Solution
4,523 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Relas 

In FreeRTOS, the stack size specified in xTaskCreate() is measured in words (not bytes). For the LPC51U68, which uses a 32-bit word size, each word is 4 bytes.
For instance, if you specify configMINIMAL_STACK_SIZE + 50, this translates to (configMINIMAL_STACK_SIZE + 50) * 4 bytes of stack space.

The alignment adjustments by FreeRTOS or the compiler can cause discrepancies between the requested stack size and the actual allocated size.

BR

Hang

View solution in original post

1 Reply
4,524 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Relas 

In FreeRTOS, the stack size specified in xTaskCreate() is measured in words (not bytes). For the LPC51U68, which uses a 32-bit word size, each word is 4 bytes.
For instance, if you specify configMINIMAL_STACK_SIZE + 50, this translates to (configMINIMAL_STACK_SIZE + 50) * 4 bytes of stack space.

The alignment adjustments by FreeRTOS or the compiler can cause discrepancies between the requested stack size and the actual allocated size.

BR

Hang