cannot find -llpc_board_nxp_lpcxpresso_1549

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot find -llpc_board_nxp_lpcxpresso_1549

1,610件の閲覧回数
athmesh_n
Contributor IV

I'm working on Modbus communication, after creating a new project and building gives me the following error

  • c:/nxp/mcuxpressoide_10.2.1_795/ide/tools/bin/../lib/gcc/arm-none-eabi/7.2.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llpc_board_nxp_lpcxpresso_1549
  • c:/nxp/mcuxpressoide_10.2.1_795/ide/tools/bin/../lib/gcc/arm-none-eabi/7.2.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llpc_chip_15xx
  • collect2.exe: error: ld returned 1 exit status
  • make: *** [MODBUS_TEST.axf] Error 1

Controller : LPC1517

IDE :   MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25]

Is there any solution ? is there anything to consider before creating the project?

Regards,

Athmesh Nandakumar

ラベル(1)
1 返信

1,444件の閲覧回数
converse
Senior Contributor V

It looks like you have created an LPCOpen project (selected during project creation) but either do not have the LPCOpen projects in your workspace, or you have not built them. Note that you need to build LPCOpen in both Debug and Release configurations, so that those equivalent configurations of your project will find the.