Hi,
I am using cJSON is a project but am having an issue building it that I don't understand.
If I include references to cJSON_Print(), then the build fails with an error message "undefined reference to __isnan". This is despite the fact that this is available to the build, in math.h (which is #included).
Why would the build fail in this way, even though the required definition/file is actually there?
thanks
-Nick
已解决! 转到解答。
I got some time to look into this, and on second glance it seemed obvious that Redlib was missing these dependencies, and changing to Newlib has fixed this. Thanks.
Exactly my point. The error message does not match the code.
Here is the code:
/* Render the number nicely from the given item into a string. */
static cJSON_bool print_number(const cJSON * const item, printbuffer * const output_buffer)
{
    unsigned char *output_pointer = NULL;
    double d = item->valuedouble;
    int length = 0;
    size_t i = 0;
    unsigned char number_buffer[26] = {0}; /* temporary buffer to print the number into */
    unsigned char decimal_point = get_decimal_point();
    double test = 0.0;
    if (output_buffer == NULL)
    {
        return false;
    }
    /* This checks for NaN and Infinity */
    if (isnan(d) || isinf(d))
    {
        length = sprintf((char*)number_buffer, "null");
    }
    else
    { ..........And here is the compiler error:
C:\mcuxpresso_workspace\sdm_01\Debug/../source/cJSON.c:562: undefined reference to `__isnand'
If I CTRL-click on the isnan in the code, then it takes me to the definition in math.h as expected.
So, why the compiler error? The code looks OK to me.
Thanks,
-Nick