.axf firmware write. can not set MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.axf firmware write. can not set MCU

1,747 Views
erik_hedberg
Contributor I

firmware download with .axf file.  can not set MCU in MCUXpresso IDE

Please direct me how

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,677 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Erik,

Hope you are doing well.

Please provide the microcontroller that you are working with.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply

1,677 Views
converse
Senior Contributor V

too little info. can't help.

0 Kudos
Reply